with S32K144 EVB board i find it only connect with pc usb port the board can power up, when connect with 5v usb adaptor , the board can't power.
How to power board with 5v usb adaptor ?
Hi
When connect with 5v usb adaptor, the MK20DX128VFM5 did not output high voltage at POWER_EN signal. So it disable 5v from USB connector.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Ok, thanks @Robin_Shen
another quesiton about i2c not work with freertos, could you help to check it
please see attached code
also i have raise ticket before, but can't resolved it
https://community.nxp.com/t5/S32K/s32k144-FreeRTOS-I2C/m-p/1677024