S32K144 Debug

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K144 Debug

2,326件の閲覧回数
zaker
Contributor I

I made a mistake that I artificially modified the PFLASH 0x00000100 address of the program data,  and the MCU keeps resetting now. I try to power reset the MCU and immediately debugged, but it is keeps resetting too. How can i resolve it

0 件の賞賛
返信
1 返信

2,301件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please try to use P&E Recovery Utility halt MCU by refer to Recovering Cortex-M Microcontroller with a Power Glitch.

For more detailed information, see the discussion here: S32K144 D2 RED LED is ON always


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信