S32K14

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K14

4,851 Views
gravity_one
Contributor III

all dear:

PROJECT : 1、freeRTos  2、power manager  3、CAN

freeRTos+power manager into POWER_STATE_VLPS mode is ok,

but add init CAN ,into POWER_STATE_VLPS is fail,and MCU is restart,why?

can you help me?

thanks

grayli

Tags (1)
0 Kudos
Reply
8 Replies

4,709 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello [email protected],

Do you put the FlexCAN module into Freeze mode before VLPS?

Thanks,

BR, Daniel

0 Kudos
Reply

4,709 Views
gravity_one
Contributor III

hi,Daniel

i add function:

void CAN_Freeze_mode(uint8_t instance,bool enable)
{
CAN_Type * base = g_flexcanBase[instance];
DEV_ASSERT(instance < CAN_INSTANCE_COUNT);
if(enable)
FLEXCAN_EnterFreezeMode(base);
else
FLEXCAN_ExitFreezeMode(base);
}

1、
into VLPS mode ,before set CAN_Freeze_mode(INST_CANCOM1,1);

but mcu restart

2、
into VLPS mode ,before set FLEXCAN_DRV_Deinit(INST_CANCOM1);
is ok,but i need CAN_IRQ wake up MCU,

3、
i need add CAN_ID filter?
FLEXCAN_DRV_ConfigRxMb(INST_CANCOM1, RX_MAILBOX, &dataInfo, 0x0);
FLEXCAN_DRV_SetRxMbGlobalMask(instance,FLEXCAN_MSG_ID_STD,0x1);
but CAN receive all ID.
Not only should you receive (CAN_ID) 0x0 and 0x1??

why is all ID?

sorry ,so much issue,I just started learning NXP MCU.

can you help me,please

thanks 

BRS

Grayli

0 Kudos
Reply

4,709 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi [email protected],

The FlexCAN module is not a wake-up source in VLPS (7.3.1 Wake-up sources, RM rev.11).
But PORT interrupts are functional in all digital pin muxing modes including CAN_RX (12.6.1 Pin Control Register n (PORT_PCRn)) and can bring the MCU from VLPS.

BR, Daniel

0 Kudos
Reply

4,709 Views
gravity_one
Contributor III

hello,Daniel

 

deinit CAN and set CAN pin to muxing mode,before into VLPS

thanks

BRS

Grayli

0 Kudos
Reply

4,709 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi [email protected],

The PORT interrupt (wake-up event) on the corresponding pin is functional in VLPS even if the FlexCAN module is initialized and the pin is routed to the CAN_RX function in PCR[MUX].

BR, Daniel 

0 Kudos
Reply

4,709 Views
gravity_one
Contributor III

hello,Daniel

i test CAN set to port interrupt can wake on MCU form sleep mode ;

but again init CAN ,MCU restart.

can you help solve why MCU restart?

 

0 Kudos
Reply

4,709 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello [email protected],

I assume that you are running the application stand-alone without any debugger connected.

So, I would place an infinite loop in the wake-up ISR (variable = 1; while(variable){}) and then attach a debugger without resetting the MCU and step the code, examine registers, check if clocks are enabled. Do you have HardFault ISR in your code implemented? 

BR, Daniel

0 Kudos
Reply

4,709 Views
gravity_one
Contributor III

hi,Daniel

thanks,into Freeze mode,CAN_IRQ can wake up  in VLPS?

BRS

grayli

0 Kudos
Reply