S32K118EVB2Q048 Board HMI Mapping and schematic

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K118EVB2Q048 Board HMI Mapping and schematic

Jump to solution
7,047 Views
AlexV32
Contributor I

Hello,

I was wondering if there is an HMI Mapping and schematic available for the S3K118 EVB 48Pin MCU version of the board? (S32K118EVB2Q048) I could only find stuff for the 64Pin MCU version (S32K118EVB-Q064) which, although similar, seems to have different header pinouts

I´m attaching a pic of the back of the board for reference.

Thanks in advance. Regards

Alex V.

0 Kudos
Reply
1 Solution
7,006 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@AlexV32

      I send it to you privately,please check it.

BR!

     Jim,

View solution in original post

0 Kudos
Reply
4 Replies
7,019 Views
AlexV32
Contributor I

Hi @Senlent,

Thanks, it seems S32K116EVB2Q048 and S32K118EVB2Q048 do share the same HMI mapping so this is very useful. 

Still, I couldn´t find the schematic for any of these two, only for their previous versions which do not have the J5 header (S32K116EVB-Q048).

I was particulary interested in the touch pads, I want to know the pin mapping to the pads. I´m working on touch button control so I want to know which MCU pins are connected to the pads circuitry.

Any info you could provide on this is highly appreciated. I´m attaching the schematic bit I´m looking for (this one is for the old board version)

Thanks! Regards

Alex V.

0 Kudos
Reply
7,007 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@AlexV32

      I send it to you privately,please check it.

BR!

     Jim,

0 Kudos
Reply
6,987 Views
AlexV32
Contributor I

Many thanks @Senlent !!

Regards

Alex V.

0 Kudos
Reply
7,034 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@AlexV32

You can refer to S32K116EVB,S32K118EVB2Q048 seems similar to S32K116EVB.

https://www.nxp.com/design/development-boards/automotive-development-platforms/s32k-mcu-platforms/s3... 

BR!

      Jim,

 

0 Kudos
Reply