S32K118 BOOTLOADER

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K118 BOOTLOADER

3,195件の閲覧回数
raviranjankumar
Contributor III

Hi,

I want to implement bootloader for s32k118 EVB. If I am flashing the code with debugger from any start address, after jumping to that address my application is running properly. But if I am writing same application hex file using FTFC then after jumping it reset the controller.

I have tested Flash read, write and erase. It is working fine. And I have disabled watchdog also. what is the issue I am not able to find?

Please help with the required information.

Thanks and regards,

Ravi Ranjan Kumar.

0 件の賞賛
返信
2 返答(返信)

2,757件の閲覧回数
raviranjankumar
Contributor III

Can anybody help me with required information..?

0 件の賞賛
返信

2,757件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Ravi Ranjan Kumar,

Sorry for the late response. I recommend you checking the application note AN12218 (link). This application note explains how to make a bootloader for the S32K. You can download the software from the following link.


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------