S32K116 touch problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K116 touch problem

1,157件の閲覧回数
taiguo_han
Contributor I

Hello!

We want to develop a steering wheel switch similar to the figure below :

无标题2.png

We want to use s32k116 MCU with the touch film(below figure)

无标题1.png

But now there is a problem :We need to put a plastic plate on the touch film. The thickness of the plastic plate is about 3mm. The touch threshold(ELEC2_TOUCH_THRESHOLD_DELTA) has been adjusted to 15, which is still not sensitive.

From the software point of view, is there any way to improve touch sensitivity? The project development time is a little urgent. Is there someone could help me?

Any suggestions are welcome. Thank you very much!

0 件の賞賛
返信
0 返答(返信)