S32K116 UART Communication protocol emulation over FLEXIO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K116 UART Communication protocol emulation over FLEXIO

3,028 Views
jayashreepasane
Contributor III

I'm trying to emulate UART over flexi on the S32116EVB developer kit. I want to keep the TX of UART by default high (open drain) and then start putting data on tx line. As explained in the reference manual I have the following bits in the register to make it supprort opendrain. 

FLEXIO-> SHIFTCTL [0] | = FLEXIO_SHIFTCTL_PINCFG (0x01);
FLEXIO-> SHIFTCTL [0] | = FLEXIO_SHIFTCTL_PINPOL (0x01);

When I do the setting as mentioned above in the register , TX line remains at low state and no communication happens (failed to transmit) 

Config_11.PNG

I want to set the state of the pin to default high. and start transmission over tx line, Currently this is not possible without external pull up resistor. required.PNG

So can anyone tell me, if it is true that I always need an external pullup register to achieve communication as given in the above picture?

I am attaching my sample setting too for tx line

clock enable

PCC-> PCCn [PCC_PORTA_INDEX] | = 1 << PCC_PCCn_CGC_SHIFT;
// PORTD_0 set as FLEXIO
PORTD-> PCR [2] | = 0x00000400; / * Port D2: MUX = FLEXIO * / 

// Enable clock to the FXIO
(PCC-> PCCn [PCC_FlexIO_INDEX]) | = 0x41000000;

FLEXIO-> CTRL | = FLEXIO_CTRL_DBGE (1);
FLEXIO-> SHIFTSTAT = 0x0F;

// TRANSMITTER
// shifter configuration
FLEXIO-> SHIFTCTL [0] | = (FLEXIO_SHIFTCTL_TIMSEL (0) | FLEXIO_SHIFTCTL_TIMPOL (0) | FLEXIO_SHIFTCTL_PINSEL (0x03) | FLEXIO_SHIFTCTL_SMOD (0x02));
FLEXIO-> SHIFTCTL [0] | = FLEXIO_SHIFTCTL_PINCFG (0x01);
FLEXIO-> SHIFTCTL [0] | = FLEXIO_SHIFTCTL_PINPOL (0x01);
FLEXIO-> SHIFTCFG [0] | = (FLEXIO_SHIFTCFG_INSRC (0) | FLEXIO_SHIFTCFG_SSTOP (0x03) | FLEXIO_SHIFTCFG_SSTART (0x02));
// set baud rate
// FLEXIO-> TIMCMP [0] = 0x00000F04;
// timer configuration
FLEXIO-> TIMCFG [0] | = (FLEXIO_TIMCFG_TIMOUT (0) | FLEXIO_TIMCFG_TIMDEC (0) | FLEXIO_TIMCFG_TIMDIS (0x02) | FLEXIO_TIMCFG_TIMENA (0x02) | FLEXIO_TIMCFG_TSTOP (0x02) | FLEXIO_TIMCFG_TSTART (0x01));

 

0 Kudos
Reply
3 Replies

2,807 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Jayashree pasane

PINCFG and PINPOL are for the logical behaves of the pin, but as long as you are using this pin as open drain, it will need a pull up to work. You can use the internall pullup of the MCU, it is enabled with the PE and PS of the PORT_PCRn field.

Hope this helps

Best regards
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

0 Kudos
Reply

2,807 Views
jayashreepasane
Contributor III

Hello Jorge,

Thank you again for the response.

I tried to enable the internal pull up, but still I face the same issue. I am trying to use Evaluation board S32K116EVB. 

Regards,

Jayashree P

0 Kudos
Reply

2,807 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi jayashree pasane

In order to have the flexIO TX of UART by default high you need to set:

FLEXIO-> SHIFTCTL [0] | = FLEXIO_SHIFTCTL_PINCFG (0x00);
FLEXIO-> SHIFTCTL [0] | = FLEXIO_SHIFTCTL_PINPOL (0x03);

With this config, you will have TX high by default and when transmission happens, it will act as your second scope.

Regards

Jorge Alcala

0 Kudos
Reply