S32K116_EVB Clock output

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K116_EVB Clock output

2,392 次查看
kwakd_y
Contributor III
I want to use clock out with S32K116_EVB.
I seted it as follows, but it does not work.
Please respond what is the problem.
void CLKOUT_init(void)
{
 PCC->PCCn[PCC_PORTB_INDEX ] |=PCC_PCCn_CGC_MASK;  /* Enable clock for PORTB */
 PTB->PDDR |= (1<<5);        /* Data Direction= output (default) */ 
 PORTB->PCR[5] |= PORT_PCR_MUX(5);             /* Port B5: MUX = CLKOUT */

SIM->CHIPCTL |= SIM_CHIPCTL_CLKOUTSEL(8);
SIM->CHIPCTL |= SIM_CHIPCTL_CLKOUTDIV(0); //Output clock divide by 1
SIM->CHIPCTL |= SIM_CHIPCTL_CLKOUTEN(1); //Enable CLKOUT
}
标记 (4)
2 回复数

2,235 次查看
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

The "SIM->CHIPCTL |= SIM_CHIPCTL_CLKOUTSEL(8); " means that you have chosen the SPLLDIV2_CLK option as CLKOUT.

However, the Phase-locked loop (PLL) is not available for the S32K11x product series.

I would like to point you to the Reference Manual rev 9. section "27.2 High level clocking diagram" note number 3.

"3. For S32K11x, inputs and muxes connected to PCC are Reserved. Also, SPLLDIVx_CLK are Reserved as indicated in RED"

Best Regards,

Diana

2,235 次查看
MarvinLiu
Contributor II

Thanks for your suggestion!

0 项奖励
回复