S32K1 MCAL_ClockSettingConfig Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K1 MCAL_ClockSettingConfig Error

Jump to solution
2,905 Views
wuxianlong
Senior Contributor I

Hi,all

Why are the system clock and SIRC clock or FIRC clock not  MCU under control together?

I configured two sets of clocks, possibly violating this rule, and the MCU occasionally has an exception (stay in reset). I suspect a problem with this configuration, but no details have been found。

 MCAL Pack: S32K1XX_ackMCAL4_2_RTM_HF3_1_0_4

wuxianlong_0-1687919207548.png

Best Regards

xianlong

 

0 Kudos
Reply
1 Solution
2,855 Views
cuongnguyenphu
NXP Employee
NXP Employee
0 Kudos
Reply
3 Replies
2,856 Views
cuongnguyenphu
NXP Employee
NXP Employee

Hi @wuxianlong ,
I found a thread with the same question as you. Please check the answer from this:
https://community.nxp.com/t5/S32K/MCU-Setting-issue-on-S32K14X-MCAL4-2-RTM-1-0-4-about-quot-Clock/m-...

 

0 Kudos
Reply
2,838 Views
wuxianlong
Senior Contributor I

this way may not aviod the  22920 bug in the release note. i am not sure the way is ok.

0 Kudos
Reply
2,819 Views
cuongnguyenphu
NXP Employee
NXP Employee

The MCAL-22920 in the release note is the bug that fixed in this version. So the workaround above would not affect to this

0 Kudos
Reply