S32K max supported ISELED

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K max supported ISELED

850 次查看
aks029
Contributor I

For POC I will be using S32K-ISELED LED Lighting Solution EVK. 

I want to understand on the  limitations related to

- max number of leds ?

- iseled stack ?

- code size ?

 license for evaluation ?

 

 

0 项奖励
回复
2 回复数

649 次查看
Chaitanyaj
Contributor I

Does S32K144-Q100 includes S32K ISELED part numbers which include the full production license? 

0 项奖励
回复

826 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @aks029 

The S32K-ISELED Application Development Kit (ADK) comes with a 16-LED bar, but the ISELED Communication Protocol can address up to 4079 LEDs.

The development kit and the non-ISELED S32K standard part number device can only be used with the the free-of-charge evaluation version of the ISELED software driver.

NOTE: Limited functionality: Mandatory driver re-initialization after 150,000 (SDK version) or 10,000 (AUTOSAR version) ISELED commands.

For production, developers should order one of the S32K ISELED part numbers which include the full production license with unlimited driver functionality. 

For more information, please contact ISELED directly or your NXP representative.

 

BR, VaneB

0 项奖励
回复