S32DS3.5 S32K344 CAN配置

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS3.5 S32K344 CAN配置

Jump to solution
1,297 Views
ZhouPengfei
Contributor III

如何使用S32DS3.5 RTD3.0.0配置CAN,正常收发数据,是否有教程。

example是loopback模式,不知道如何改成正常模式

0 Kudos
Reply
1 Solution
1,217 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @ZhouPengfei 

Please check the following example. This is not configured in loopback mode, which might be useful to you. 

Example S32K344 FlexCAN_Ip TX/RX/EnhanceRXFIFO test S32DS3.4 RTD200

View solution in original post

0 Kudos
Reply
4 Replies
1,227 Views
ZhouPengfei
Contributor III

@VaneB 

Hello VaneB,

Do there any help?

0 Kudos
Reply
1,281 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @ZhouPengfei 

To not generate any misunderstanding. Could you please help me by writing your question in English? 

 

B.R.

VaneB

0 Kudos
Reply
1,259 Views
ZhouPengfei
Contributor III

Hi @VaneB ,

Thanks for your help.

I have one board of S32K344, I want to test CAN with PTA 6/7 as CAN0, PTC 10/11 as CAN5.

The CAN transmit chip is TJA1044GT

I create a project based on Can_Example_S32K344, configured the pin and Port. I alse disable the loopback mode of example.

But when I debug it, it no data.

I am wondering is there something wrong for my configuration or I called wrong API.

The attachment is my test project.

Thanks for your help again.

0 Kudos
Reply
1,218 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @ZhouPengfei 

Please check the following example. This is not configured in loopback mode, which might be useful to you. 

Example S32K344 FlexCAN_Ip TX/RX/EnhanceRXFIFO test S32DS3.4 RTD200

0 Kudos
Reply