S32DS3.5 Complier setting

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS3.5 Complier setting

891 Views
Hanoch
Contributor II

Hello NXP colleagues, 

I don't konw why I can't complie it after I imported a new example demo.

Hanoch_0-1728211413776.png

as you can see, the console shows so many faults. bascilly, most of faults belongs to "no such file or directory". Do I need to add them to the Path Setting one by one??? Why I can't add a Path Folder, The IDE can't search the header files automatically?

 

my tool Chain Editor:

Hanoch_1-1728211770136.png

 

The Build Varables:

Hanoch_2-1728211800060.png

 

the SDKs:

Hanoch_3-1728211814356.png

 

 

Tags (1)
0 Kudos
Reply
1 Reply

865 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @Hanoch,

Have you tried to update the code? When importing a project, not all the files are generated yet, so it is needed to open Config Tools, and click "Update Code":

Julin_AragnM_1-1728316634719.png

 

Julin_AragnM_2-1728316638961.png

Best regards,
Julián

 

 

0 Kudos
Reply