Error in final launch sequence
Failed to execute MI command:
thbreak main
Error message from debugger back end:
Cannot access memory at address 0x4b8
Cannot access memory at address 0x4b8
when I debuged my project,why is this a problem?
how can I do it?
Hello,
Could you please provide more information about the behavior you are facing? For example, are you using one of our evaluation boards? If so, which one? Are you trying to debug one of the SDK examples? If so, which one? What version of S32DS are you using?
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------