S32 Design Studio for S32 Platform 3.4 ⇒ Open Projects from file system.... Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 Design Studio for S32 Platform 3.4 ⇒ Open Projects from file system.... Issue

1,437件の閲覧回数
autics
Contributor III

I compiled the program normally using the S32 Design Studio for S32 Platform 3.4.

It also runs well.

The problem is that when I open the project again as below, it is empty at some point.

STEP1.png

 

STEP2.png

0 件の賞賛
返信
2 返答(返信)

1,415件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @autics 

Does the project still appear in your workspace file (location path example, C:\Users\workspaceS32DS.3.4)? According to the shared images, the project already exists in the workspace, the possible cause is that you deleted the project on S32DS but did not delete the contents on disk.

 

BR, VaneB

0 件の賞賛
返信

1,342件の閲覧回数
autics
Contributor III

Hi @VaneB

Sorry for the late reply,

there was a mail verification error and I solved it with NXP remote help for a few days.

I deleted all the data in the C:\***\workspace S32DS.3.4 space,

but it doesn't work the same way.

In addition, I think I deleted all the project creation files from other workplaces, but they still don't work.

 

0 件の賞賛
返信