S32 Configuration Tools S32K3 R1.8 NPI download not available

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Configuration Tools S32K3 R1.8 NPI download not available

1,842 Views
Christina_
Contributor I

Hello,

I've got a problem to find Configuration Tools S32K3 R1.8 NPI for the S32K344 in the DS Extensions. There are just Configuration Tools available for S32K36x, S32K37x and S32K39x derivatives.

My Design Studio version is 3.6.0 and I also installed S32K3 RTD R21-11 Version 5.0.0.

Any suggestions how to resolve?

Thanks!

0 Kudos
Reply
7 Replies

1,822 Views
PavelL
NXP Employee
NXP Employee

Hello @Christina_ ,

It looks like that you haven't installed S32K3xx development package. Please double check also that S32K3xx RTD is installed:

PavelL_0-1759746310501.png

Best regards,

Pavel

0 Kudos
Reply

1,800 Views
Christina_
Contributor I

Hello @PavelL ,

thanks for your reply. S32K3xx development package is installed as well as S32K3xx RTD. This can't be the cause of the missing extension.

Best regards

Christina

 

0 Kudos
Reply

1,791 Views
Christina_
Contributor I

Are the "S32 Configuration Tools S32K3 R1.8 NPI data packages for S32K3" included in the "S32 Configuration Tools Package" yet?

DSConfigToolsExt.PNG

 

0 Kudos
Reply

1,783 Views
PavelL
NXP Employee
NXP Employee

Hello @Christina_ ,

Thank you for sharing all the data.

I apologize, I missed your very first question.

There's no dedicated Configuration Tools S32K3 R1.8 NPI for the S32K344. 

Please check that you can see S32K344 in the new S32DS application project wizard:

PavelL_0-1759830359458.png

Also, you should see S32K344 examples in Create S32DS Project from example wizard:

PavelL_1-1759830547366.png

Best regards,

Pavel

0 Kudos
Reply

1,779 Views
Christina_
Contributor I

Hello @PavelL , yes there I can see the S32K344

0 Kudos
Reply

1,775 Views
PavelL
NXP Employee
NXP Employee

Hello @Christina_ ,

Thank you for your confirmation. So, everything appears to be correct.

Best regards,

Pavel

0 Kudos
Reply

1,722 Views
Christina_
Contributor I

Hello @PavelL ,

yes it seems that it was now integrated in the S32 Configuration Tools Package.

Thank you for your replys!

Best regards

Christina

0 Kudos
Reply