Running Flex CAN with internal clock problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Running Flex CAN with internal clock problem

1,229件の閲覧回数
swati_jha
Contributor I

Hi everyone we are using s32k148 microcontroller we have running CAN application ,

please provide some reference code for FLEXCAN using SIRC clock source .

ラベル(1)
0 件の賞賛
返信
1 返信

1,169件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello, Swati Jha

SIRC clock cannot be used as the FlexCAN oscillator clock. FlexCAN oscillator clock is SOSCDIV2_CLK as mentioned in Table 27-9 of the reference manual. 


Have a great day,
Victor

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信