Resetting S32k14x

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,511件の閲覧回数
aungkm
Contributor III

Hi, 

I accidentally flashed s32k14x with s32k11x example in the MBDT and I am having trouble flashing the s32k14x again.

Is there any solution to solve this?

タグ(2)
0 件の賞賛
返信
1 解決策
2,505件の閲覧回数
aungkm
Contributor III

Hi Robin,

P&E Recovery Utility did the trick.

Thanks!

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,507件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Did P&E Recovery Utility work? https://community.nxp.com/t5/S32K/Can-t-use-PEmicro-debugger-with-S32K118EVB2-Q048/td-p/1376204

Have you tried MSD Flash Programmer?

Get Started with the S32K144EVB.pngGet Started with the S32K144EVB.png

Or Select the Emgerency Kinetis Device Recovery by Full Chip Erase.

Robin_Shen_0-1631865841507.pngRobin_Shen_0-1631865841507.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
2,506件の閲覧回数
aungkm
Contributor III

Hi Robin,

P&E Recovery Utility did the trick.

Thanks!

0 件の賞賛
返信