Reprogramming an existing 0 bit to an existing 0 in Flash memory

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reprogramming an existing 0 bit to an existing 0 in Flash memory

Jump to solution
1,937 Views
El-Mohr
Contributor I
I am using NXP S32K148 and am trying to change one bit in a flash page from 1 to 0 without erasing the page. Problem is that this will require writing 0s on existing 0s in the same phrase, which according to the reference manual is not allowed as it overstresses the device.
 
My questions are:
1- Does "not allowed" mean I can't do it, like it wouldn't be performed by hardware or it's doable but not advised?
2- If it's doable, what does it mean to "overstress the device", or to what extent should I be concerned knowing that I will do that only once?
 
Thanks
0 Kudos
Reply
1 Solution
1,929 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

overstress is not the only thing to consider. Next important point is ECC. Each phrase has hidden ECC syndrome which is programmed to the flash at the same time as data. If you are going to overwrite the phrase, new ECC syndrome corresponding to new data is calculated and ECC is programmed again. And it may be necessary to change '0' in old ECC syndrome to '1' which doesn't work, of course. It can lead to single or multiple bit ECC error.

So, it is possible to overwrite non-erased phrase but it's not recommended. And because this was not characterized, we can't give you guarantees.

Regards,

Lukas

 

View solution in original post

1 Reply
1,930 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

overstress is not the only thing to consider. Next important point is ECC. Each phrase has hidden ECC syndrome which is programmed to the flash at the same time as data. If you are going to overwrite the phrase, new ECC syndrome corresponding to new data is calculated and ECC is programmed again. And it may be necessary to change '0' in old ECC syndrome to '1' which doesn't work, of course. It can lead to single or multiple bit ECC error.

So, it is possible to overwrite non-erased phrase but it's not recommended. And because this was not characterized, we can't give you guarantees.

Regards,

Lukas