Report a bug in S32K144 EAR_0.8.4 SDK function SMC_SetPowerMode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Report a bug in S32K144 EAR_0.8.4 SDK function SMC_SetPowerMode

1,386 次查看
justinsheng
Contributor II

A bug in SDK EAR_0.8.4 has been detected (in power_smc_hw_access.c), which will halt the CPU if DEV_ASSERT is enabled:

status_t SMC_SetPowerMode(SMC_Type * const baseAddr,

                          const smc_power_mode_config_t * const powerModeConfig)

{

........ 

/* Previous code: */

    /*DEV_ASSERT((((uint16_t)SMC_GetPowerModeStatus(baseAddr)) & transitionTable[powerModeName]) != 0U);*/

/* Should be logic AND, not bit AND */

    DEV_ASSERT((((uint16_t)SMC_GetPowerModeStatus(baseAddr)) && transitionTable[powerModeName]) != 0U);

}

Hope NXP can fix it in the next SDK release.

标签 (1)
标记 (3)
0 项奖励
回复
0 回复数