Reception supported through both Rx FIFO and individual buffer at same instance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reception supported through both Rx FIFO and individual buffer at same instance

1,453 Views
chandru_v
Contributor I

Hi,

In S32K148, is reception supported through both Rx FIFO and individual buffer at same instance.

For Example:

-> I will enable FIFO.

-> 0-10 buffers are provided for FIFO reception.

-> 11-15 are provided for dedicated reception, will hardware try to find a match in 11-15 buffers if reception doesn't pass through FIFO filters.

0 Kudos
Reply
1 Reply

1,392 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

yes. this is possible.

You can refer to simple example on https://community.nxp.com/docs/DOC-343091 

BR, Petr 

0 Kudos
Reply