RUNING CAN FD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RUNING CAN FD

1,564 Views
Palawut
Contributor I

Hi there

I am writing to inquire about S32K14xseries (S32K142 and S32K146) if I am going to change form using CAN to CAN FD. Is it usable ? ( both of them ) or What needs to be changed or add something?  such as Circuit  Connectors (  Software and hard ware ) 

I am looking forward to hearing from you soon. Thank you

0 Kudos
Reply
3 Replies

1,552 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Palawut

1.S32K-RM Chapter 55.1.1 Instantiation information

Senlent_2-1645611086870.png

be careful about the flexcan instance differences between S32K142 and S32K146,

 

2.and the CAN transceiver needs to support CAN FD.

 

0 Kudos
Reply

1,532 Views
Palawut
Contributor I

Thank for your answer 

So
1.can i make sure that we dont need to replace pin and connectors
2.We need to use specific software  (Coding) to use CAN FD
3. Is  this possible to find out that it can run CAN FD definitely? (coding online)

could you suggest me

0 Kudos
Reply

1,517 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Palawut

1.for some package, the s32k146 is a pin-to-pin compatible superset of S32K142, so I would say yes for your first question.

2.you need to do some special configuration for CAN FD, and you can use loop-back to test the CAN module.

I don't quiet understand the last two questions your asked, but I hope this answer can help you.

0 Kudos
Reply