RMII interface with 25MHz?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RMII interface with 25MHz?

1,385件の閲覧回数
FSeliger
Contributor I

I am using S32k together with a SJA1105 Ethernet switch. Between these deviced, I have inverted the Clock-Signals, so that I can not generate the 50MHz clock with the MCU.
I could generate 25MHz with the SJA1105.

Is it possible to run the RMII interface with 25MHz clock?

Thanks!

0 件の賞賛
返信
1 返信

1,368件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

I don't think so, 50MHZ is needed for RMII mode.

BR, Petr

0 件の賞賛
返信