Hi
FTFC_FOPT[RESET_PIN_CFG] can be used to disable the RESET_b function. But: there could be a short period of contention during a POR ramp where the MCU drives the pin low prior to establishing the setting of this option and releasing the reset function on the pin.
It is not recommended to use the RESET_b pin as a normal IO port.
![FTFC_FOPT[RESET_PIN_CFG].png FTFC_FOPT[RESET_PIN_CFG].png](https://community.nxp.com/t5/image/serverpage/image-id/163135iA4B221057DE2F858/image-size/large?v=v2&px=999)
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------