RD-BESS1500BUN BMS Monitor GUI no data

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RD-BESS1500BUN BMS Monitor GUI no data

3,230 Views
bev
Contributor I

Hello,

I have:

  • RDBESS772BJBEVB
  • RDBESS774A1EVB - 1 CMU
  • RD-BESSK358BMU
  • BATT-18EMULATOR

I have used the BMS Monitor GUI as per video/instructions, except I have selected 1 CMU mode. (please see attached photo). 

BMU has been flashed with S32K3-BESS-Firmware-Version-0.8.0 Firmware via JLink.

I seem to get no data in BJB and CMU measurements tab  -  I can see TempBMU.

Is Single CMU mode not supported?

Please see attached screenshot and log from script.

Is internal comm fault relevant? 

 

InternalError = {
SFTY_MGR_FAULT_UNINTENDED_CONNECTION =  0 ,
SFTY_MGR_FAULT_UNINTENDED_DISCONNECTION =  0 ,
SFTY_MGR_FAULT_INTERNAL_COMM =  1 ,
SFTY_MGR_FAULT_SUPPLY_VOLTAGE =  0 ,
SFTY_MGR_FAULT_DC_LINK_FUSE =  0
}

 

 

0 Kudos
Reply
1 Reply

3,176 Views
RafaR
NXP Employee
NXP Employee

Hi bev

Okay, please check the hardware connections for both the CMU and BJB with the bmu, and make sure the battery emulator is powered with the suitable adapter (5V and 3A or 4A). 

I hope this information has helped you, Please let me know your results.

 

Have a great day and best of luck.

0 Kudos
Reply