RD-BESS1500BUN BMS Monitor GUI no data

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RD-BESS1500BUN BMS Monitor GUI no data

3,190件の閲覧回数
bev
Contributor I

Hello,

I have:

  • RDBESS772BJBEVB
  • RDBESS774A1EVB - 1 CMU
  • RD-BESSK358BMU
  • BATT-18EMULATOR

I have used the BMS Monitor GUI as per video/instructions, except I have selected 1 CMU mode. (please see attached photo). 

BMU has been flashed with S32K3-BESS-Firmware-Version-0.8.0 Firmware via JLink.

I seem to get no data in BJB and CMU measurements tab  -  I can see TempBMU.

Is Single CMU mode not supported?

Please see attached screenshot and log from script.

Is internal comm fault relevant? 

 

InternalError = {
SFTY_MGR_FAULT_UNINTENDED_CONNECTION =  0 ,
SFTY_MGR_FAULT_UNINTENDED_DISCONNECTION =  0 ,
SFTY_MGR_FAULT_INTERNAL_COMM =  1 ,
SFTY_MGR_FAULT_SUPPLY_VOLTAGE =  0 ,
SFTY_MGR_FAULT_DC_LINK_FUSE =  0
}

 

 

0 件の賞賛
返信
1 返信

3,136件の閲覧回数
RafaR
NXP Employee
NXP Employee

Hi bev

Okay, please check the hardware connections for both the CMU and BJB with the bmu, and make sure the battery emulator is powered with the suitable adapter (5V and 3A or 4A). 

I hope this information has helped you, Please let me know your results.

 

Have a great day and best of luck.

0 件の賞賛
返信