RAppID bootloader S32K144 

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RAppID bootloader S32K144 

2,122 次查看
yogesh_khedkar
Contributor I

Hello Community,

I'm new user of s32k1xx series controller. Im using the s32k Design studio and i was trying the sample SDK example given in the IDE. When i was trying RAppID bootloader S32K144 i was getting the following error while starting the bootloader...

pastedImage_2.png

pastedImage_1.png

I have modified the .rbl file and updated the .srec path, i'm following the procedure mentioned in the .rbl file.....

I have connected my EVB with OpenSDA ...

pastedImage_3.png

Any suggestions or help will be appreciated.... :-)  

标签 (1)
0 项奖励
回复
2 回复数

1,997 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

did you tried cycle power of the board as is suggested in error message? There is timeout in Bootloader app. The communication  should be started shortly after Board is powered up (not sure about delay value - it is probably something like 10 sec). 

Jiri

0 项奖励
回复

1,997 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

due to nature of serial-to-USB bridge, my recommendation is to reset the device by reset button only. Do not do power-off / power-on sequence. This could help.

Regards,

Lukas

0 项奖励
回复