Query regarding impact on AFE if AFE VBAT_PWR pin filter capacitance changed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Query regarding impact on AFE if AFE VBAT_PWR pin filter capacitance changed

1,591 Views
varunbharti
Contributor III

Hi, 

I am using MC33774A for our LV BMS application for two-wheelers and three-wheelers. Due to system interference, we are experiencing a 2-usec dip on VBAT_PWR, which is causing the AFE to reset. (I have attached the recommended schematic and oscilloscope snip for reference)
To solve this issue, we want to decrease the cutoff frequency of the RC filter on VBAT_PWR by increasing the value of Cpwr to 0.47uF from 0.1uF.
In the datasheet, it is mentioned not to change the Cpwr value, but we don't see any impact on increasing the value.
Can anyone please verify and list the impact of increasing the value of  Cpwr from 0.1uF to 0.47uF

 

MC33774  

0 Kudos
Reply
3 Replies

1,556 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

This capacitor can be increased up to 4.7µF, see AN12963, section 5.4 - SM03 accuracy. Then 0.47µF is ok.

BRs, Tomas

0 Kudos
Reply

1,545 Views
varunbharti
Contributor III
The AN12963 hardware guideline is recommended for MC33771x and MC33772x, but we are using MC33774A.
0 Kudos
Reply

1,514 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

Please accept my apologies for this mistake, I will update this thread as soon as I have the answer for the MC33774A, still checking internally.

BRs, Tomas

0 Kudos
Reply