Problem with run S32K14X_MCAL4_0_RTM_1_0_3_Sample_Application

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem with run S32K14X_MCAL4_0_RTM_1_0_3_Sample_Application

2,674 Views
maciej_cebula
Contributor II

Hi, 

I have evalBoard S32K144EVB-Q100 and I want to run S32K14X_MCAL4_0_RTM_1_0_3_Sample_Application.

I am using the EB tresos 25.1.0. 

The first problem which occured is already when I want to import the project I got

"Plug-in with a module "EcuC_TS_T40D2M10I3R0" is not installed - cannot create module configurations for project "kinetis" " 

pastedImage_1.png

I watch the plugins folder and there is missing this module. Should I remove this module and go on with tresos configuration?

Next my question if is possible to run Sample Application in S32 Design Studio for ARM

Version: 2018.R1 to build project and debug through OPENSDA? 

Best regards Maciej. 

0 Kudos
Reply
2 Replies

2,498 Views
martin_kovar
NXP Employee
NXP Employee

Hello Maciej,

I created case for automotive software team in our internal system and I sent them your question. They will contact you back directly via email.

Please let me know, if you do not receive any answer until end of the week.

Regards,

Martin

0 Kudos
Reply

2,498 Views
maciej_cebula
Contributor II

hi Martin

thanks a lot:)

0 Kudos
Reply