Problem with bootloader S32K344

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem with bootloader S32K344

1,342 Views
JonAnder_Amante
Contributor II

Hi, 

I am using the project "S32K344_Can_bootloader_RTD200" in the microprocessor S32K344. I want to download an application with the program of bootloader. I have achieved the jump from program to application but I have different questions.

1. I want to use #define EN_DELAY_TIME but when I uncomment the command in the folder "public_inc", the program has different errors. My target to use "Backdoor", that is to say, I want to check if the program has to enter to bootloader or not. I don´t know the process and the different functions that I have to use to achieve the target. I want to use the function "Boot_CheckReqBootloaderMode(void)" but when I debug the program, it never enters to the "if". Could you explain me the process and the steps to achieve the target. I add different functions that I think are important. 

2. I don´t know if I have to modificate the parameters of "static tJumpAppDelayTimeInfo gs_stJumpAPPDelayTimeInfo = {FALSE, 0u};". I have to change this structure ? You can see all structure in one of the next pictures. 

I need the reply as soon as possible since I have to send a project very soon. 

JonAnder_Amante_0-1711018826640.png

JonAnder_Amante_1-1711019080742.png

JonAnder_Amante_0-1711019413360.pngJonAnder_Amante_1-1711019429904.png

JonAnder_Amante_2-1711019456137.png

 

Thank you for all, 

Jon Ander Amante Jorge

 

 

0 Kudos
Reply
2 Replies

1,324 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @JonAnder_Amante 

I’m sorry to say that Unified bootloader shared on the community is only unofficial demo provided AS IS with no guarantees and no support. Currently we do not have resources to support this demo. We apologize for any inconvenience.

Regards,

Lukas

0 Kudos
Reply

1,308 Views
JonAnder_Amante
Contributor II

Hi,

A few days ago you send me different advices about this project. I don´t know how to solve the problem and I need to send the project very soon. I hope you reply as soon as possible. 

Thank you for all,

Jon Ander Amante Jorge

0 Kudos
Reply