Problem with S32K3X4EVB-T172

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem with S32K3X4EVB-T172

1,147 Views
JonAnder_Amante
Contributor II

Hi,

 

I have different problems with my S32K3X4EVB-T172. When I try to load to project I can´t load correctly. I have always 3 leds on (D2, D14, D15 and D21). The chip FS25 is heating so much (the jumper 18 is on positicion as in the photo)  and I don´t know if I have to change Fs26 o chip S32K344. Could yoy give information about this and if I can change. 

JonAnder_Amante_0-1761130303093.png

 

 

Thank you

0 Kudos
Reply
3 Replies

1,122 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @JonAnder_Amante,

Most likely the MCU has been damaged, causing VDD_HV_A_MCU to short to GND and FS26 to heat up. It has been discussed in this other community post: Solved: Re: S32K358 EVB Not working - NXP Community.

You can try switching the MCU mounted on the board.

Best regards,
Julián

0 Kudos
Reply

1,105 Views
JonAnder_Amante
Contributor II

Hi,

Could you give a price about how much can it cost to change the microprocessor and where I can ask?

 

Thank you

0 Kudos
Reply

1,086 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @JonAnder_Amante,

Prices will depend on availability in your region. I'm not familiar with specific businesses which do these procedures, but you will probably need to contact one who provide SMT (Surface-Mount Technology).

Best regards,
Julián

0 Kudos
Reply