Powering S32K144 EVB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Powering S32K144 EVB

1,742件の閲覧回数
chris4iot
Contributor I

I am planning to use 12v 1.5Amp Adapter? Can you please suggest power rating limits of S32K144 EVB

タグ(2)
1 返信

1,668件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

this is not specified because it depends also on external loads. But if we consider that max current consumption of the microcontroller is roughly 60mA, current consumption of rest of the board won't be more than a few tens of mA. And if you connect some external circuits to the pin headers than it also won't be so significant. In this case, adapter 12V/1.5mA is more than enough.

Regards,

Lukas