Ping Not Responding Using lwIP FreeRTOS Example on S32K344 Mini EVB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ping Not Responding Using lwIP FreeRTOS Example on S32K344 Mini EVB

93 Views
brunoGT88
Contributor III

I am using the lwip_FreeRTOS_s32k344 example as a reference for Ethernet communication on the S32K344 Mini EVB board.

However, the ping from the PC to the board is not responding. We are using RTD version 5.0.0 and NXP TCPIP Stack version 2.0.0.

At this point, we would like to understand if there is any additional configuration required for this example to work correctly, such as PHY configuration, clock settings, pin configuration, IP address settings, or any specific changes needed for the S32K344 Mini EVB.

Could you please help us identify what may be missing or incorrectly configured?

0 Kudos
Reply
0 Replies