Peripheral tool code generation error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Peripheral tool code generation error

1,815件の閲覧回数
TWL
Contributor III


When I use S32DS for Platform 3.5 update (8) to configure a project for the S32K312 chip, after configuring peripherals and clicking to update the code, it shows errors with peripherals and clock. However, I'm using the default project, the clock hasn't been configured yet, and the peripherals are set to default values. The RTD version for S32K312 is 3.5.13.20240726.

TWL_0-1746511646458.pngTWL_1-1746511664975.png

 

0 件の賞賛
返信
4 返答(返信)

1,790件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Even for newly created S32K312 project, there are default configurations in the Clocks Tool. Please enable code generation for Clocks.

S32 Configuration Tool Clocks.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

1,772件の閲覧回数
TWL
Contributor III

The following image shows my operation. When I created a new project, I opened all code generation tools, and when I clicked update code, the following error was displayed.

TWL_0-1746670488449.png

TWL_1-1746670512020.png

 

 

0 件の賞賛
返信

1,769件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

First of all, I see that you installed S32K3 RTD 3.0.0 P01. But now it has been updated to 5.0.0. If it is a new project, it is recommended to use the latest version of RTD.
I did not encounter this error when creating a new project with S32DS v3.5 + RTD 3.0.0 P07. If you insist on using S32K3 RTD 3.0.0, then I suggest you uninstall this S32DS v3.5 and refer to this article to reinstall it HOWTO: offline install S32K3 RTD 3.0.0 in S32DS v3.5

 

Best Regards,
Robin

0 件の賞賛
返信

1,748件の閲覧回数
TWL
Contributor III

Hi

I followed the steps you provided, but I'm still encountering the issue mentioned above.

TWL_0-1746681772011.png

 

0 件の賞賛
返信