PMSM motor parameters

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PMSM motor parameters

1,016件の閲覧回数
ZooTech
Contributor I

In the S32K344 BLDC/PMSM Development Kit | NXP Semiconductors following application could you specify the motor parameters of the specified PMSM motor like stator resistance, Ld, Lq and so on ?

0 件の賞賛
返信
2 返答(返信)

992件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

The devkit info and the examples can be found here:

https://www.nxp.com/design/design-center/development-boards-and-designs/MCSPTE1AK344

and

https://community.nxp.com/t5/S32K-Knowledge-Base/S32K3-Motor-control-SW-examples/ta-p/1804577

regarding the motor:

Low-Cost PM motor—3-phase PM motor equipped with Hall sensor, 24 VDC, 9000 RPM, 95 W, 42BLY3A78-24110  

petervlna_0-1748598015224.png

The parameters can be found in MCAT in application in the tab "parameters".

Best regards,

Peter

0 件の賞賛
返信

998件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Let me ask motor control team and I will come back to you ASAP.

Best regards,

Peter

0 件の賞賛
返信