PIT TRGMUX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PIT TRGMUX

931 Views
enthuCutlet
Contributor II

I have 8 channels configured on ADC0 and 3 channels configured on ADC1. Can I use one PIT channel(PIT0 CH0) to trigger 2 TRGMUX hardware input which in turn trigger ADC0 and ADC1 respectively. Will this start parallel conv of ADC0 and 1. 

enthuCutlet_0-1701156644195.png

enthuCutlet_1-1701156690150.png

 

 

0 Kudos
Reply
1 Reply

909 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

I have configured TRGMUX on S32K1 to select the same Hardware Input for two different Hardware Output. So I think this is also feasible on S32K3.
You can test if it works.


Best Regards,
Robin

0 Kudos
Reply