PDB trigger input source

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PDB trigger input source

1,516 Views
anita_tranzillo
Contributor I

Hi all, I have a question about the external trigger source for PDB-ADC peripheral.

At pag. 1182 of S32K manual, I read:

"...A trigger input event is defined as a rising edge being detected on a selected
trigger input source…."

I would like to know if there is the possibility to generate a trigger also when a falling edge is detecte.

Thanks a lot

0 Kudos
Reply
1 Reply

1,467 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hi anita tranzillo,

 

Unfortunately, in the section 44.4.1 PDB pre-trigger and trigger outputs only explains how to use the rising edge and in the registers doesn't explain how to change the polarity.

 

Best Regards,

Alexis Andalon

0 Kudos
Reply