PDB - ADC back to back triggering (S32K micro)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PDB - ADC back to back triggering (S32K micro)

3,770件の閲覧回数
tsugiart
Contributor I

Hello,

I attempt to trigger ADC via PDB in back to back fashion.  

I have read other link on how to do this. The link provides an example where 

initial trigger is performed by software trigger. However, I would like to perform

the initial trigger by trigger delay from PDB.  I can't get it to work with my 

PDB configuration. Below, is some of relevant PDB configuration that I think 

is critical.  Basically, I try to trigger 2 A2D channel (Ch0 and Ch1 of ADC0).

Ch0 is triggered by pre-trigger delay of PDB, Ch1 is triggered after it receives

COCO flag from Ch0  (back to back). 

 

...

SIM_CHIPCTL[PDB_BB_SEL] = 0;

PDB0->MOD = 950;

PDB0->CH[0].C1 |   =   PDB_C1_BB(0b00000010) //Pretrigger Back to Back: 0= disabled, 1=enabled
                                       | PDB_C1_TOS(0b00000001) //Pretrigger Output Select: 0=bypassed , 1=enabled
                                       | PDB_C1_EN(0b00000001); //Pretrigger Enable: 0=enabled , 1=enabled

PDB0->CH[0].DLY[0] = 200;

 

The behavior that I see is in the debugger, Ch0 of ADC0 seems get triggered. 

It generates COCO flag, however Ch1 of ADC0 doesn't seem to respond to COCO flag 

from Ch0.  

 

Thank you in advance for your help.

 

Tanto

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,799件の閲覧回数
tsugiart
Contributor I

Hi All,

I found out the problem is with sequence in which initialization of ADC and PDB configuration

is being called in my main code.  In my main code, PDB initialization is called before ADC.

The ADC initialization routine that I have contains auto-calibration.

Once I comment out the auto-calibration part from my ADC initialization,  or swap ADC and PDB

initialization, my program runs just fine.  

I suspect auto-calibration of ADC might run longer than one PDB period (maximum count on PDB as specified by

PDB->MOD).  I am not quite clear behavior of S32 micro, when PDB goes over several cycles when ADC

doesn't get a chance to respond to previous pre-trigger.  Is it simply just reporting the error to PDB->CHnS

register, or it will do something about it.

Thanks,

Tanto 

0 件の賞賛
返信

2,799件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi Tanto,

Yes, the PDB.CHnS[ERR[m]] gives a feedback about wrong trigger sequence. A sequence error typically happens because the delay m is set too short and the pre-trigger m asserts before the previously triggered ADC conversion finishes.

BR, Petr

0 件の賞賛
返信