P&E Debug session closed for S32K358

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P&E Debug session closed for S32K358

1,067 Views
soumik1506
Contributor III

Hello Experts,

Since Last week, i have trying to flash one of my projects into my custom built S32K258 Board using the P&E micro multi link interface with a J-TAG connection. Till last Thursday, i was able to load the project into the board.

Once i added the lines for my free-master application, i was getting error messages stating that debugger could not find the .elf file of the project.

I made sure that the debug configuration were the basic settings for a DEBUG_FLASH. I did not change anything. I was getting the same elf file error.

Later, i tried flashing the project in to the board in Release_FLASH mode. The program loaded once, i was able to test it. But, when i try to flash the updated program, i am getting the following error in the debugger console...

 

soumik1506_0-1731947298154.png

I updates the debugger drivers in my S32DS IDE and tried flashing my program, no luck. Same error

i tried flashing other programs to check if this specific to my program, but still no luck. I am getting different error messages in the debugger console log. Is there any why to recover the s32K358 board.

Soumik

Tags (2)
0 Kudos
Reply
1 Reply

1,034 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

there is probably missing .elf file for boot core (M7_0_0) . 

0 Kudos
Reply