Output voltaje thersholds versus Source Current

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Output voltaje thersholds versus Source Current

2,581 Views
DiegoRC
Contributor I

Hello.

I need to know the logical digital output thresholds of the S32K1xx series, based on the current supplied for the range of VDD = 3.3V.

Already consulted the Table 17- Datasheet (S32K-DS) but they are only specified for certain currents (3mA-3.5mA to VDD = 3.3V) , as well as the Figure 8 - AN2434 that only specifies it for VDD = 5V.

0 Kudos
Reply
4 Replies

2,573 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Specified Voh/Vol is min/max value when sourcing/sinking current is Ioh/Iol as specified.
V-I characteristic for logic 1 (output) can estimated by linear approximation between points and <Ioh;Voh> and <0mA ; VDD>. The same way you can estimate V-I characteristic for logic 0.

0 Kudos
Reply

1,238 Views
seanli_study
NXP Employee
NXP Employee

Hi David:

     Does the S32K1 have the threshold data for VOL and VOH? If it depends on the sourcing/sinking current? Can VOL_max be calculated through the formula of MOS transistor's resistance * sink maximum current? Can we obtain this data?

0 Kudos
Reply

2,567 Views
DiegoRC
Contributor I

Hello. Thanks for the support.

For an estimate it seems valid to me. But not for a "worst-case analysis" (as is my case).

Is it the only theoretical way to get the thresholds?

Is there no such data?

0 Kudos
Reply

2,557 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

How it is defined (i.e. minimum current at defined voltage) it is basically worst case.

You can also use IBIS model we are providing.

0 Kudos
Reply