Output current on IO pins vs the number of enabled IOs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Output current on IO pins vs the number of enabled IOs

727 Views
reham
Contributor I

Hello,

I'm using NXP S32K142,

Will the output current differ on micro-controller pin  incase more pins are set as output high ?

In other words, setting 2 pins as OUTPUT HIGH vs setting 6 pins as OUTPUT HIGH.

as I noticed that in case of setting 6 pins the total amount of charge is less.

your quick feedback is highly appreciated.

Thanks,

0 Kudos
Reply
1 Reply

721 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi reham,

Please refer the IOHT in "Table 19. DC electrical specifications at 5.0 V Range for S32K1xx series" of S32K1xx MCU Family - Data Sheet.

IOHT.pngBest Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply