OTA using UDS over LIN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OTA using UDS over LIN

3,369 Views
PradeepM
Contributor I

Hi,

There is a requirement of OTA using UDS over LIN communication.

Device: S32K144EVB evaluation board.

S32DS: S32 Design Studio for ARM--Version: 2018.R1

SDK :S32SDK_S32K14x_RTM_2.0.0

I have downloaded unified_bootloader_demo_V2.1 

I'm using the below path UDS Example code in S32K144EVB.

D:\PDLC\unified_bootloader_demo_V2.1\unified_bootloader_demo_v2.1\S32K1xx\S32K144_LIN\S32K144_LIN_bootloader

 

In Readme file its mentioned like :Run Import_stack.bat for import UDS and porting folder in the Sources 

when I try to run Import_stack.bat I am getting error as shown in screenshot(Import error).

 

Apart from this I have tried compiling S32K144_LIN_bootloader directly but I am not able to build the code .Please find the error screenshot (build error).

Please do the needful to address the issue. Thanks in advance.

 

 

 

 

0 Kudos
Reply
1 Reply

3,338 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @PradeepM,

I’m sorry to say that Unified bootloader shared on the community is a demo only provided AS IS with no guarantees and no support.

Currently we do not have resources to support this demo.

We apologize for the inconvenience.

 

Regards,

Daniel

0 Kudos
Reply