OPENSDA Development Guide and Bootloader

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OPENSDA Development Guide and Bootloader

1,709件の閲覧回数
asrikrishnagovind
Contributor II

Hello, in the PDF: OpenSDA on TWR-KW2x Users Guide (nxp.com), in page-3 it says "OpenSDA applications can be found in the OpenSDA Developer’s Guide (available October 2012)". Where can I find this PDF?

And based on the schematics of S32K144-Q100, if one were to duplicate the schematics of the same and make a prototype, what are the basic programs that are to be loaded into the OpenSDA's microcontroller, and the main Microcontroller of the S32K144-Q100 Board? And how would one do the same? Thanks and regards.

0 件の賞賛
返信
1 返信

1,696件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi asrikrishnagovind,

The version of OpenSDA on S32K1xx EVB are V1. I am afraid you can not clone it.

Here are some related question from P&E Micro forum:
OpenSDA
Program/Debug issue with S32K142-Q48
OpenSDA solution for MPC5748G on custom hardware
If you still have questions, you can contact P&E Micro for consultation.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信