Not able to flash through OPENSDA

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Not able to flash through OPENSDA

2,279件の閲覧回数
ambarishhundeka
Contributor III

Hello,

I am using S32K144 evaluation board.

power up the board and flashing through USB .

Earlier I was able to do flashing, but now not able to flash.
The red led next to the USB stays on, and the board will not enter boot loader mode when powered with reset button pressed.


RGB LEDS are continuously glowing but not able to connect to the board via OpenSDA Interface.

I clicked on the debug in S32 design studio , Open SDA window opens and ask for the Open SDA USB port , if I click on Retry also , again and again it is asking the same (Retry option).


Thank you in advance for your help.



Regards,
Ambarish 









ラベル(1)
1 返信

2,015件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi Ambarish,

The LED D1 next to the USB indicate reset and when the board is in reset the RGB LED should not glowing.

It is hard to detect how your issue occurs because I’m not sure what is your setting on your board and how you supply the board.

For example, the board could be damaged in the case when jumper setting is set for the power supply from micro USB

and 12 V power supply is connected together with micro USB power supply to the board.

Best regards,

Diana