Not able to do Mass Erase using ULINK2 debugger

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Not able to do Mass Erase using ULINK2 debugger

1,618 次查看
prabhatg44
Contributor I

Hello Team,

I deactivated SWD interface of S32K116 MCU by configuring FSEC register. During this process, I have enabled Mass erase for doing further development work but after 3-4 times interface is not able to do Mass erase. Can you please support how to unlock the device.

Please find snapshots for your reference.

prabhatg44_0-1626099806611.pngprabhatg44_1-1626099824007.pngprabhatg44_2-1626099839700.png

 

0 项奖励
回复
1 回复

1,598 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi prabhatg44,

Please try to use the P&E Recovery Utility described in Recovering Cortex-M Microcontroller with a Power Glitch.

Notice that a debug probe from PEMICRO is needed.(can not use ULINK2 debugger or J-Link debugger) If you are using S32K116EVB, then the onboard OpenSDA can be used.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复