No Flash Operation After Power-Up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No Flash Operation After Power-Up

1,085 Views
Andy_B
Contributor I

I am using a PEmicro Multilink to develop and flash code into my target board with IAR Embedded Workbench.  This works fine when the debugger is connected, and I get a UART prompt and some flashing LEDs (to let me know the firmware is running).

If I remove the debugger and cycle power the code does not appear to work: no UART prompt and no flashing LEDs.  

When flashing I get the warning below, so I assume that I've got something improperly set in either my linker command file or project settings.  Most of the code I'm using, at least for start-up, is from NXP's RTD (version 4.4.2.0.0) for the processor I'm using.

Andy_B_0-1670965285117.png

Any insight into how to resolve this would be appreciated.  Thank you in advance.

 

0 Kudos
Reply
1 Reply

1,069 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Andy_B,

Looks more related to IAR, please contact IAR's technical support. I'm not familiar with the use of IAR, but maybe you can refer to this: https://www.iar.com/knowledge/support/technical-notes/general/creating-a-bootloader-for-cortex-m/
Also, have you tried the 'Attach to Running Target' feature to see where the program goes wrong?


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply