Need full RTD source package and decouple example for FRDM-S32K344 — India developer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need full RTD source package and decouple example for FRDM-S32K344 — India developer

265 Views
ashwin95raghavan
Contributor I

Hello NXP team,

I have FRDM-S32K344 with S32DS 3.6.6. I have a working
dual-core project on S32K328 with RTD 7.0.0 and want to
use S32K344 in decoupled dual-core mode.

Two requests:

1. Full RTD source package for S32K344 — Package Manager
only shows DS_updatesite.zip, not full source tree.

2. Access to Example_S32K344_decouple_RTD400_Ip_C40_DS35
project to write UTEST DCF record (LOCKSTEP_EN=0).

My UTEST address 0x1B000780 is blank and verified ready.

Board: FRDM-S32K344
IDE: S32DS 3.6.6
Debugger: PE Micro onboard
Location: India

Please advise or connect me to India FAE.
Thank you.

 

RTD/LOCKSTEP/NXPS32K344

 

0 Kudos
Reply
1 Reply

249 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

1) once you add/install RTD updatesite within S32DS, the RTD source code is visible within S32DS installation folder, e.g. 
c:\NXP\S32DS.3.6.5_RTD700\S32DS\software\PlatformSDK_S32K3\RTD
Also you have a possibility to download standalone RTD version. Within NXP Automotive Package Manager if you selecetd whole RTD package it would contain *.exe file as well (e.g. SW32K3_S32M27x_RTD_R23-11_7.0.0_QLP03_D2512.exe , which is a standalone installation, usable for Tresos usage etc.
This is also available from your SW library account https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K3-STDSW-D
Go to Automotive SW - S32K3/S32M27x - Real-Time Drivers for Cortex-M  and select the RTD version you need.
 
2) The project you mentioned can be downloaded directly from 
 
BR, Petr
0 Kudos
Reply