Mismatch between the PIN configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Mismatch between the PIN configuration

1,414 Views
harish93
Contributor I

Hi,

Could you please help me to figure out this issue:

When I am referring the excel file (S32K148_IO_Signal_Description) attached to the Reference Manual for Port Configuration of this particular parameter (PortPin Pcr ) in EB tresos tool. As per the IO signal Table sheet the pin we need to configure is Pin 15 for CAN Rx channel but in tresos if I configure the PortPin Pcr as 15 we are unable to select the PortPin Mode as CAN0_Rx and it is same for the CAN0_Tx Mode for Pin 14 in tresos.

Please find the attachments.

IO_Signal.pngTresos.png

0 Kudos
Reply
1 Reply

1,391 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

Seems that you configure the wrong PortPin Pcr. Please read the AUTOSAR_MCAL_PORT_UM.pdf.
PORTE4 PortPin Pcr=128+4=132
PORTE5 PortPin Pcr=128+5=133

PortPinPcr AUTOSAR_MCAL_PORT_UM S32K1.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply