Memory Protection for Dual core S32k322 Controller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Memory Protection for Dual core S32k322 Controller

1,700 Views
Lisha
Contributor III

Hi Team,

Could you please share any example project or reference material demonstrating the use of MPU (Memory Protection Unit) and PPU (Peripheral Protection Unit) for a dual-core setup on the S32K322 controller?

BR,

Lisha

Tags (1)
0 Kudos
Reply
4 Replies

1,678 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

The S32K322 does not include a module named 'PPU'. If you're referring to peripheral access protection, this is managed through the XRDC (Extended Resource Domain Controller), which allows you to configure access rights for peripherals and memory regions across the dual-core setup. Let us know if you were referring to a different concept or platform.

Example code you may find within RTD:

davidtosenovjan_1-1747741262600.png

RM_Example.. shows also XRDC setup example, Platform_.. contains MPU setup example

 

0 Kudos
Reply

1,570 Views
Lisha
Contributor III

Hi @davidtosenovjan ,

Thank you for the reference to the MPU example. However, I couldn't find an MPU example specifically for a dual-core setup. Could you please assist me with this?

BR,

Lisha 

Tags (1)
0 Kudos
Reply

1,475 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

There is no such example. Basically as multi-core projects are done separately for each core, and MPU is peripheral of the core, you would use two such projects. Configuration is however application specific.

0 Kudos
Reply

1,667 Views
Lisha
Contributor III

Thank You @davidtosenovjan I look into that

 

BR,

Lisha

0 Kudos
Reply