McuPeripheralClockConfig has not enough children

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

McuPeripheralClockConfig has not enough children

2,477 Views
gediz
Contributor I

Hello,
We are trying to walk through the demo application that Tresos provided us by default called simple_demo_can_rte. When we were at the Update BSW and SWC description wizard step we encountered an error called McuPeripheralClockConfig has not enough children says "It has 34 child - allowed are 41 to 41 child. The children are ..."

Note: We selected our board which is s32k148_lqfp176 in the dropdown located in the Resource_TS_T40D2M10I2R0 (ResourceSubderivative).

When we selected the demo's default resourceSubderivative (s32k146_lqfp100) no errors occurred.

But in the boards folder (of simple_demo_can_rte project) which is located inside the source folder there is a default folder named FRDMK144_Q100_SCOS. This board is member of s32k144 family right? I am confused that when I select the s32k144_lqfp100 the same error occurred but with different child numbers.

Do you have any suggestion regarding McuClockSettingConfig error. For instance, adding the missing children? (We don't know what to add for s32k148_lqfp176)

0 Kudos
Reply
1 Reply

2,420 Views
cuongnguyenphu
NXP Employee
NXP Employee

Which SW version your're using, I see the spanshot is so weird, ANd how did you take this Simple_demo_can_rte?

The missing children can be added by click on the Plus button and select missing peripheral clock:

cuongnguyenphu_0-1694594749013.png

 

0 Kudos
Reply