MWCT2016 HSE 2.40.0 Secure Boot Configuration Failure- ImportPlainSymKeyReqMuChannel

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MWCT2016 HSE 2.40.0 Secure Boot Configuration Failure- ImportPlainSymKeyReqMuChannel

741 Views
ShrikantM
Contributor I

Environment

  • MCU: MWCT2016S based Wireless Charging Controller
  • Working Setup (Legacy):
    • HSE FW Version: 2.6.0
    • (Application + Secure Boot) merge hex.
  • New Setup (Failing):
    • HSE FW Version: 2.40.0
    • (Application + Secure Boot) merge hex.

We are migrating from HSE FW v2.6.0 to HSE FW v2.40.0 while maintaining the same Qi key provisioning and Secure Boot flow.

Problem Statement

With HSE FW v2.6.0, the complete provisioning sequence executes successfully:

  1. HSE installation
  2. Erase Keys
  3. S2TP key slot provisioning
  4. Qi key programming
  5. Secure Boot configuration
  6. Application boots successfully

 

With HSE FW v2.40.0, all provisioning steps complete successfully until Secure Boot configuration is started.

During Secure Boot configuration the following API fails:

ImportPlainSymKeyReqMuChannel() in secure boot code.
 
return HSE response: 0x55A5A399 which corresponds to: 
#define HSE_SRV_RSP_INVALID_PARAM ((hseSrvResponse_t)0x55A5A399UL)
 
After this failure, Secure Boot configuration cannot be completed, and the ECU remains stuck in the Secure Boot code.
 

Provisioning Sequence

Working Configuration (HSE 2.6.0)

00_Blank_MWCT2016_CodeFlash_DataFlash.hex
Power Reset
01_HSE_flash.srec  version 2.6.0
Power Reset
02_EraseKeysSW.hex
Power Reset
03_S2TP_KeySlotsAligned.srec  S2TP SW Version: 1.1.1
Power Reset
Write Qi Keys via UART
Power Reset
Application+SecureBoot.hex
Power Reset
 
 
HSE response after merge hex flashing from UART log:
 HseStatus : 2848
        bit 0   : 0 RFU
        bit 1   : 0 HSE_SHE_STATUS_SECURE_BOOT
        bit 2   : 0 HSE_SHE_STATUS_SECURE_BOOT_INIT
        bit 3   : 0 HSE_SHE_STATUS_SECURE_BOOT_FINISHED
        bit 4   : 0 HSE_SHE_STATUS_SECURE_BOOT_OK
        bit 5   : 1 HSE_STATUS_RNG_INIT_OK
        bit 6   : 0 HSE_STATUS_HOST_DEBUGGER_ACTIVE
        bit 7   : 0 HSE_STATUS_HSE_DEBUGGER_ACTIVE
        bit 8   : 1 HSE_STATUS_INIT_OK
        bit 9   : 1 HSE_STATUS_INSTALL_OK
        bit 10  : 0 HSE_STATUS_BOOT_OK
        bit 11  : 1 HSE_STATUS_CUST_SUPER_USER
        bit 12  : 0 HSE_STATUS_OEM_SUPER_USER
        bit 13  : 0 HSE_STATUS_FW_UPDATE_IN_PROGRESS
        bit 14  : 0 RFU
        bit 15  : 0 RFU
 smrCoreStatus_Get :
 smrCoreStatus[1] : 0 , smrCoreStatus[0] : 0
 smrStatus[1] : 0 , smrStatus[0] : 0
 
Code debug log HSE response:
 ImportPlainSymKeyReqMuChannel-hseResp: 0x55a5aa33
 
 LoadBootMacKey-hseResp: 0x55a5aa33
 
 Generic_ImportKeys-hseResp: 0x55a5aa33
 
 KeyProvisioningForJTAG-status: 1
 
 SecureBootConfiguration-hseResp: 0x55a5aa33
 
 KeyProvisioningToHseNVM-status: 1
 
 NON_SECURE_IVT-BLOCK1-hseResp: 0x55a5aa33
 
 SECURE_IVT-BLOCK0-hseResp: 0x55a5aa33
 
 writeDefaultData
 
 Running Secure Boot CFG program
 Hse-FW Version : 0.13.0.2.6.0 , full mem
 using interface version : 0.13.0.2.6.0
 HseStatus : 2862
        bit 0   : 0 RFU
        bit 1   : 1 HSE_SHE_STATUS_SECURE_BOOT
        bit 2   : 1 HSE_SHE_STATUS_SECURE_BOOT_INIT
        bit 3   : 1 HSE_SHE_STATUS_SECURE_BOOT_FINISHED
        bit 4   : 0 HSE_SHE_STATUS_SECURE_BOOT_OK
        bit 5   : 1 HSE_STATUS_RNG_INIT_OK
        bit 6   : 0 HSE_STATUS_HOST_DEBUGGER_ACTIVE
        bit 7   : 0 HSE_STATUS_HSE_DEBUGGER_ACTIVE
        bit 8   : 1 HSE_STATUS_INIT_OK
        bit 9   : 1 HSE_STATUS_INSTALL_OK
        bit 10  : 0 HSE_STATUS_BOOT_OK
        bit 11  : 1 HSE_STATUS_CUST_SUPER_USER
        bit 12  : 0 HSE_STATUS_OEM_SUPER_USER
        bit 13  : 0 HSE_STATUS_FW_UPDATE_IN_PROGRESS
        bit 14  : 0 RFU
        bit 15  : 0 RFU
 smrCoreStatus_Get :
 smrCoreStatus[1] : 0 , smrCoreStatus[0] : 0
 smrStatus[1] : 1 , smrStatus[0] : 1

 

Failing Configuration-HSE FW 2.40.0 reports:
00_Blank_MWCT2016_CodeFlash_DataFlash.hex
Power Reset
01_S32K344_HSE_FW_UPDATE_v2_40_0.srec
Power Reset
02_M210WLCUMBCD00A_WSB00.31_EraseKeySW_UART_ENABLE.hex
Power Reset
03_S2TP_2_1_0_KeySlotsAligned.srec
Power Reset
Write Qi Keys via UART
Power Reset
Application+SecureBoot.hex
Power Reset
 
 HseStatus : 2912
        bit 0   : 0 RFU
        bit 1   : 0 HSE_SHE_STATUS_SECURE_BOOT
        bit 2   : 0 HSE_SHE_STATUS_SECURE_BOOT_INIT
        bit 3   : 0 HSE_SHE_STATUS_SECURE_BOOT_FINISHED
        bit 4   : 0 HSE_SHE_STATUS_SECURE_BOOT_OK
        bit 5   : 1 HSE_STATUS_RNG_INIT_OK
        bit 6   : 1 HSE_STATUS_HOST_DEBUGGER_ACTIVE
        bit 7   : 0 HSE_STATUS_HSE_DEBUGGER_ACTIVE
        bit 8   : 1 HSE_STATUS_INIT_OK
        bit 9   : 1 HSE_STATUS_INSTALL_OK
        bit 10  : 0 HSE_STATUS_BOOT_OK
        bit 11  : 1 HSE_STATUS_CUST_SUPER_USER
        bit 12  : 0 HSE_STATUS_OEM_SUPER_USER
        bit 13  : 0 HSE_STATUS_FW_UPDATE_IN_PROGRESS
        bit 14  : 0 RFU
        bit 15  : 0 RFU
 smrCoreStatus_Get :
 smrCoreStatus[1] : 0 , smrCoreStatus[0] : 0
 smrStatus[1] : 0 , smrStatus[0] : 0
ImportPlainSymKeyReqMuChannel-hseResp: 0x55A5A399
 
after Power reset:
 UML SW Version : WSB00.3B_UART_ENABLE
 
 Running Secure Boot CFG program
 Hse-FW Version : 0.13.0.2.40.0 , full mem
 using interface version : 0.13.0.2.40.0
 
 HseStatus : 2848
        bit 0   : 0 RFU
        bit 1   : 0 HSE_SHE_STATUS_SECURE_BOOT
        bit 2   : 0 HSE_SHE_STATUS_SECURE_BOOT_INIT
        bit 3   : 0 HSE_SHE_STATUS_SECURE_BOOT_FINISHED
        bit 4   : 0 HSE_SHE_STATUS_SECURE_BOOT_OK
        bit 5   : 1 HSE_STATUS_RNG_INIT_OK
        bit 6   : 0 HSE_STATUS_HOST_DEBUGGER_ACTIVE
        bit 7   : 0 HSE_STATUS_HSE_DEBUGGER_ACTIVE
        bit 8   : 1 HSE_STATUS_INIT_OK
        bit 9   : 1 HSE_STATUS_INSTALL_OK
        bit 10  : 0 HSE_STATUS_BOOT_OK
        bit 11  : 1 HSE_STATUS_CUST_SUPER_USER
        bit 12  : 0 HSE_STATUS_OEM_SUPER_USER
        bit 13  : 0 HSE_STATUS_FW_UPDATE_IN_PROGRESS
        bit 14  : 0 RFU
        bit 15  : 0 RFU
 smrCoreStatus_Get :
 smrCoreStatus[1] : 0 , smrCoreStatus[0] : 0
 smrStatus[1] : 0 , smrStatus[0] : 0
 
 ImportPlainSymKeyReqMuChannel-hseResp: 0x55a5a399

 

ECU getting stuck in secure boot only

0 Kudos
Reply
10 Replies

708 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @ShrikantM 

Could you please share your key catalogs as well as the parameters used in the ImportPlainSymKeyReqMuChannel() function call? The reported error indicates that one or more HSE request parameters are invalid.

 

BR, VaneB

0 Kudos
Reply

649 Views
SwapnilGawade
Contributor II

Hi @VaneB ,

We are using below key catalogs:

/* Table containing NVM key catalog entries */

const hseKeyGroupCfgEntry_t aHseNvmKeyCatalog[] =

{

    /* NvmKeyGroup_0 */

    {(HSE_MU0_MASK), HSE_KEY_OWNER_CUST, HSE_KEY_TYPE_SHE, 1U, 128U, {0U, 0U}},

    /* NvmKeyGroup_1 */

    {(HSE_MU0_MASK), HSE_KEY_OWNER_CUST, HSE_KEY_TYPE_ECC_PAIR, 1U, 256U, {0U, 0U}},

    /* NvmKeyGroup_2 */

    {(HSE_MU0_MASK), HSE_KEY_OWNER_CUST, HSE_KEY_TYPE_AES, 1U, 256U, {0U, 0U}},

    /* Marker to end the key catalog */

    {0U, 0U, 0U, 0U, 0U, {0U, 0U}}

};

 

/* Table containing RAM key catalog entries */

const hseKeyGroupCfgEntry_t aHseRamKeyCatalog[] =

{

    /* RamKeyGroup_0 */

    {(HSE_MU0_MASK), HSE_KEY_OWNER_CUST, HSE_KEY_TYPE_SHE, 1U, 128U, {0U, 0U}},

    /* Marker to end the key catalog */

    {0U, 0U, 0U, 0U, 0U, {0U, 0U}}

};

 

For below function we receive HSE_SRV_RSP_INVALID_PARAM

hseSrvResponse_t Generic_ImportKeys(void)

{

    hseSrvResponse_t srvResponse = HSE_SRV_RSP_GENERAL_ERROR;

 

    /*Import key linked with SMR#0*/

    srvResponse = ImportPlainSymKeyReqMuChannel(

            MU0,

            1U,

            NVM_AES128_BOOT_KEY,

            HSE_KEY_TYPE_AES,

            ( HSE_KF_USAGE_VERIFY ),

            0U,

            aesEcbKeyLength,

            aesEcbKey,

            TRUE

            );

    ASSERT(HSE_SRV_RSP_OK == srvResponse );

    if(HSE_SRV_RSP_OK != srvResponse)

            goto exit;

 

    /* load keys for SHE secure boot */

    srvResponse = LoadBootMacKey();

    ASSERT(HSE_SRV_RSP_OK == srvResponse );

    if(HSE_SRV_RSP_OK != srvResponse)

            goto exit;

exit:

    return srvResponse;

}

Please check attached global_defs.h for more details about the parameters.

 

Thanks and Regards,

Swapnil Gawade

0 Kudos
Reply

629 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @SwapnilGawade 

Thank you for sharing the information. Based on your configuration, I have the following observations:

  1. The SHE key group is configured with HSE_KEY_OWNER_CUST as the owner. However, the HSE Service API Reference Manual specifies that, for an SHE key catalog configuration, the owner of an SHE key group must be set to HSE_KEY_OWNER_ANY. This is also demonstrated in the NVM SHE Key Catalog Configuration example.
  2. The targetKeyHandle passed to ImportPlainSymKeyReqMuChannel() is defined as:
    #define NVM_AES128_BOOT_KEY  GET_KEY_HANDLE(HSE_KEY_CATALOG_ID_NVM, 1, 1)​
    However, according to your NVM key catalog configuration, the AES key group is the third group (NvmKeyGroup_2). Based on this configuration, the correct definition for NVM_AES128_BOOT_KEY should be: 
    GET_KEY_HANDLE(HSE_KEY_CATALOG_ID_NVM, 2, 0)​
0 Kudos
Reply

593 Views
SwapnilGawade
Contributor II

Hi @VaneB ,

As per your suggestion I have done the changes, but it also gives similar response as HSE_SRV_RSP_INVALID_PARAM (0x55a5a399).

After debugging we found that it, in ImportPlainSymKeyReqMuChannel(...)->EraseKeyReq(targetKeyHandle, HSE_ERASE_NOT_USED))->HSE_Send(muIf, muChannelIdx, gSyncTxOption, pHseSrvDesc)->Hse_Ip_ServiceRequest(u8MuInstance, u8MuChannel, pHseIp_Request , HSE_DTCM_ADDR(pHseSrvDesc))->Mu_Ip_SetTxRegister(Hse_Ip_apMuBase[u8MuInstance], u8MuChannel, (uint32)pHseSrvDesc) retruns response as HSE_SRV_RSP_INVALID_PARAM (0x55a5a399).

The parameters of pHseSrvDesc are added in attached Mu_Ip_SetTxRegister-pHseSrvDesc.xlsx.

SwapnilGawade_0-1790682414414.png

 

Thanks and Regards,

Swapnil Gawade

0 Kudos
Reply

584 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @SwapnilGawade 

According to your description, I noticed that you appear to have combined the DemoApp framework with the Hse_Ip drivers. Is my understanding correct? If so, what modifications have been applied?

Also, have you disabled the data cache in your project? This is a common cause of the HSE_SRV_RSP_INVALID_PARAM error. All data objects used for communication with HSE must be forced to non-cacheable memory.

I also noticed that you are passing HSE_DTCM_ADDR(pHseSrvDesc) as the pHseSrvDesc parameter to the Hse_Ip_ServiceRequest() function. Please refer to the thread HSE_ReadAdkp returning HSE_SRV_RSP_INVALID_ADDR, where my colleague explains some considerations regarding the use of HSE with DTCM memory.

You may also want to take a look at Hse_Ip_ToAHBAddress(), which converts a local address into an HSE host address when TCM support is enabled. It could be useful in this scenario.

0 Kudos
Reply

337 Views
SwapnilGawade
Contributor II

Hi @VaneB ,

In working setup with HSE 2.6.0 we are using following libraries:

1. RTD AUTOSAR 4.4

2. Key catalog as below

/* Table containing NVM key catalog entries */

const hseKeyGroupCfgEntry_t aHseNvmKeyCatalog[] =

{

    /* NvmKeyGroup_0 */

    {(HSE_MU0_MASK), HSE_KEY_OWNER_CUST, HSE_KEY_TYPE_SHE, 1U, 128U, {0U, 0U}},

    /* NvmKeyGroup_1 */

    {(HSE_MU0_MASK), HSE_KEY_OWNER_CUST, HSE_KEY_TYPE_ECC_PAIR, 1U, 256U, {0U, 0U}},

    /* NvmKeyGroup_2 */

    {(HSE_MU0_MASK), HSE_KEY_OWNER_CUST, HSE_KEY_TYPE_AES, 1U, 256U, {0U, 0U}},

    /* Marker to end the key catalog */

    {0U, 0U, 0U, 0U, 0U, {0U, 0U}}

};

 

/* Table containing RAM key catalog entries */

const hseKeyGroupCfgEntry_t aHseRamKeyCatalog[] =

{

    /* RamKeyGroup_0 */

    {(HSE_MU0_MASK), HSE_KEY_OWNER_CUST, HSE_KEY_TYPE_SHE, 1U, 128U, {0U, 0U}},

    /* Marker to end the key catalog */

    {0U, 0U, 0U, 0U, 0U, {0U, 0U}}

};

 

Same RTD AUTOSAR 4.4 and Key catalog we are using with HSE 2.40.0, but we are facing issue. ImportPlainSymKeyReqMuChannel(...) function returns HSE Response as HSE_SRV_RSP_INVALID_PARAM.

Hse_Ip_ToAHBAddress() function is not available in this RTD AUTOSAR 4.4.

 

Thanks and Regards,

Swapnil Gawade

0 Kudos
Reply

306 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @SwapnilGawade 

As mentioned, the SHE key group is configured with HSE_KEY_OWNER_CUST as the owner. However, the HSE Service API Reference Manual specifies that, for an SHE key catalog configuration, the owner of an SHE key group must be set to HSE_KEY_OWNER_ANY.

Have you disabled the data cache in your project? This is a common cause of the HSE_SRV_RSP_INVALID_PARAM error. All data objects used for communication with HSE must be forced to non-cacheable memory.

Also, would it be possible to share a simple example showing all the steps you are performing to import the key?
0 Kudos
Reply

229 Views
Bhushan1312
Contributor I

Hello @VaneB , 

We corrected the Key CatLog as per your suggestion and application requirements.

Secure boot works well if we are using S2TP ver1.1.0 or skipping S2TP flashing. Please see below table to get more idea. We doubting that something has changed with S2TP ver2.1.0 where CatLog is changed for Qi key import which is not matching with below Key CatLog which we have configured.

HSE VersionS2TP VersionResult
2.401.1.11. Secure Boot works
2. 25 Watt charging fails -> Qi Key import fails
Auth: Init Error: 5, Auth: Init Error - Certificate Import/Validate Failed
2.402.1.01. Secure Boot fails at Import Keys ERROR: 0x55A5A399
2. 25 Watt charging works without Secure Boot SW (Stand alone application)
3. Secure boot works if we skip S2TP flashing. But Charging functionality do not work

 

Flashing FlowErase SW: Erase and Format Key Catlog
 ↓
 Power Cycle
 ↓
 Flash Qi keys with S2TP
 ↓
 Power Cycle
 ↓
 Flash SECBoot Code: Keys Import
 ↓
 Flash Boot + App code

 

Key CatLog: 

/* Table containing NVM key catalog entries */
const hseKeyGroupCfgEntry_t aHseNvmKeyCatalog[] =
{
    /* NvmKeyGroup_0: For implicit SHE Functional operations */
    {(HSE_MU0_MASK), HSE_KEY_OWNER_ANY, HSE_KEY_TYPE_SHE, 12U, 128U, {0U, 0U}},
    /* NvmKeyGroup_1: Configured as AES to satisfy NVM_AES128_BOOT_KEY (Group 1, Slot 1) */
    {(HSE_MU0_MASK), HSE_KEY_OWNER_CUST, HSE_KEY_TYPE_AES, 4U, 128U, {0U, 0U}},
    /* NvmKeyGroup_2: Expanded to 3 slots for PROVISION_KEY0 (Slot 0) and APP_MAC_KEY (Slot 2) */
    {(HSE_MU0_MASK), HSE_KEY_OWNER_CUST, HSE_KEY_TYPE_AES, 4U, 256U, {0U, 0U}},
    /* HMAC key */ \
    { HSE_ALL_MU_MASK, HSE_KEY_OWNER_CUST, HSE_KEY_TYPE_HMAC,          2U,        HSE_KEY512_BITS, {0U, 0U} }, \
    /* ECC keys */ \
    { HSE_ALL_MU_MASK, HSE_KEY_OWNER_CUST, WRP_KEY_TYPE_ECC_PAIR,      4U,         WRP_ECC_KEY_SIZE, {0U, 0U} }, \
    { HSE_ALL_MU_MASK, HSE_KEY_OWNER_CUST, WRP_KEY_TYPE_ECC_PUB,       2U,         WRP_ECC_KEY_SIZE, {0U, 0U} }, \
    { HSE_ALL_MU_MASK, HSE_KEY_OWNER_CUST, WRP_KEY_TYPE_ECC_PUB_EXT,   1U,         WRP_ECC_KEY_SIZE, {0U, 0U} }, \
    /* RSA keys */ \
    { HSE_ALL_MU_MASK, HSE_KEY_OWNER_CUST, HSE_KEY_TYPE_RSA_PAIR,      2U,         HSE_KEY4096_BITS, {0U, 0U}}, \
    /* NvmKeyGroup_8: Explicit RSA Public Key Group for NVM_RSA2048_PUB_CUSTAUTH_HANDLE0 */
    {(HSE_MU0_MASK), HSE_KEY_OWNER_CUST, HSE_KEY_TYPE_RSA_PUB, 1U, 2048U, {0U, 0U}},
    /* Marker to end the key catalog */
    {0U, 0U, 0U, 0U, 0U, {0U, 0U}}
};
 
/* Table containing RAM key catalog entries */
const hseKeyGroupCfgEntry_t aHseRamKeyCatalog[] =
{
    /* RamKeyGroup_0 */
    {(HSE_MU0_MASK), HSE_KEY_OWNER_ANY, HSE_KEY_TYPE_SHE, 1U, 128U, {0U, 0U}},
    /* Marker to end the key catalog */
    {0U, 0U, 0U, 0U, 0U, {0U, 0U}}
};

 

Key Import failure in SecBoot code with S2TP ver2.1.0:

Bhushan1312_1-1791530834733.png

 

Bhushan1312_0-1791530803165.png

#define NVM_AES128_BOOT_KEY                     GET_KEY_HANDLE(HSE_KEY_CATALOG_ID_NVM, 1, 1)

 

 

0 Kudos
Reply

201 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Bhushan1312 

Let's try to isolate the issue first. I have sent you, in a private message, a simple demo that imports an AES-128 key, erases it, and then imports it again. Although the example is not based on the RTD version you are currently using, it should still serve as a useful reference.

Please adapt the demo to your setup and verify whether the basic key import and erase operations work correctly. This will help us align on a known working baseline and analyze the issue starting from the most basic functionality. From there, we can identify what is causing the HSE to return HSE_SRV_RSP_INVALID_PARAM in your application.

0 Kudos
Reply

108 Views
Bhushan1312
Contributor I

@VaneB Thank you for your kind support. The issue is been resolved with NXP team support.

We identified that there was issue with Key CatLog configured in S2TP SW used to import Qi keys. Its rectified now.

With this change now Secure boot working fine and also the Charging functionality works ok.

0 Kudos
Reply